Other Parts Discussed in Thread: PGA309, PGA309EVM-USB
Hi
I have the PGA309EVM-USB and USB-DAQ hardware. I'd like to use the DAQ to calibrate my own sensor hardware which uses the PGA309.
I noticed that the DAQ controls the TEST input to the PGA309 on the EVM board, which is pulled up on the DAQ board.
Reading the PGA309 documentation it says that the TEST pin should be grounded for normal operation, but pulled high to allow an external uC to write to the registers. Does this mean if I want to let the DAQ program my PGA309, I need to connect the DAQ to my PGA309's TEST pin or can the PGA309 be calibrated with the TEST pin grounded?
Regards
Bob