Other Parts Discussed in Thread: OPA381
Hello,
I am using the OPA381 to build a transimpedance amplifier for a calibrated photodiode from Thorlabs. The signal I am measuring is currently 1 kHz, but I may need to measure something as fast as 10 kHz, and in the extreme 50 kHz. The amp can be found here, and the photodiode here. I am trying to build a circuit just like the ones in Figure 1, 3, or 4 of the datasheet found here. I will need to do some experimentation to find out if I need a pull down resistor and/or a reverse bias, so I'm not sure which one of those circuits I'll use in the end.
I was able to use another TI document titled "Compensate Transimpedance Amplifiers Intuitively" to select a feedback resistor and compensation capacitor, but I'm pretty lost on picking a power supply. I'm a chemical engineer by training, so I don't know a lot about circuit design or electronics in general.
I was thinking about using this power supply because it is dual output +/- 5V, and I could experiment with a pull down resistor if necessary. Then I read that switch mode power supplies are very noisy, and I started looking at a linear +5V, +12V, -5V found here. I was looking at the HTAA-16W-AG in particular. Since it is triple output, I could run the op amp, bias the photodiode, and use a pull down resistor all from one power supply. Since it's linear instead of switching it should result in less noise as well. It's more expensive, though.
At this point I read something about by-pass capacitors in this document, and I got lost. I don't know what bypass capacitors are, or how to properly select them, or when they are necessary.
So here are my questions:
Is there anywhere I can read about properly selecting bypass capacitors for a given power supply?
In Figure 1 it shows a 1 uF capacitor on the positive side of the op amp power supply, is this a bypass capacitor? Should I just assume that I will always need to put a 1 uF capacitor there even though it isn't shown in Figures 3 or 4?
Would either of the power supplies that I have linked above work? Would I need bypass capacitors for them?
Is there another power supply that TI recommends that would be better?
Finally, and this is on a topic other than power supplies. If I were to use a big feedback resistor, say 10 MOhm, would I have any difficulty measuring the voltage output? Most multimeter leads are 10MOhm impedance, which is on the same order of magnitude. Would I end up pushing a lot of current through the leads instead of through the circuit? Should I try to find 1 GOhm leads? How should I go about measuring the voltage on the output of the op amp if I use a large value feedback resistor?
I would eventually like to hook up a BNC plug to this circuit and measure the voltage using a DAQ card on a computer. Would I run into difficulty with a high value resistor?
I realize that this is probably below the technical level of most of the people on this forum, but I really appreciate any help you can offer. I'm a bit lost and don't know where else to turn.
Thanks a lot,
-Warren