Other Parts Discussed in Thread: INA149, TINA-TI
Hi!
I use INA149 and/or AD629 in my design - see schematics.
I've experienced gain>1 (actually it was about 2) for input signal ~ 330kHz (+-200mV). I've done test without loading the output with the same gain @ 330kHz.
It could be caused by a high capacitive load, but there is only very short track with R13 unsoldered, so there's no reason for a high parasitic capacity.
OpAmp input is directly connected to a signal generrator with 50Ohm impedance.
Have anybody experienced similar behaviour of INA149 or AD629?
Thanks