Other Parts Discussed in Thread: LMH6504, TINA-TI, LMH6505
To Whom It Concerns,
The LMH6504 output oscillated when the input is near threshold. I built a bread board with the LMH6504device and the supply rails are +vc at +5 and -vc at -5v and decoupled with 25uF in parallel with 0.1uF on both rails. Rg is 100 Ohms and Rf is 10K Ohms with an input signal of +/- 10 mV. I have utilized the TINA simulator with good results. Could someone please give me some ideas as to what could cause this oscillation?
Regards, Mike Handy