This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[INA169] Using INA169 to measure 200A

Other Parts Discussed in Thread: INA169

Dear Sir

I would like to measure current with INA169 from my system with the following specifications: Imax = 200A; Vmax = 55V. The desired full-scale output voltage is 5V (ADC input). I'm using a 0.25mOhm shunt resistor (two 0.5mOhm resistors in parallel) and a 100kOhm RL resistor.

When i had make my first tests i notice that the output voltage is around 11V when I have a input current is only 3A.

Have any solution could to solve my problem?

Thanks

======================================================
I'm using the following components:
  * INA169
  * RS: 2 x 0.5mOhm (10W, 1%)
  * RL: 100kOhm (250mW, 0.1%)
  * CL: 0.1uF (output filter)