Hi. Do the 2274 op-amps have reverse polarity protection ? Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hal,
Do you mean whether the op amp has anti-phase reversal circuitry or back-to-back input protection diodes? Perhaps you should explain what is it that you are attempting to do that concerns you? Also, please clearify the op amp model name - there is no OPA2274.
Hello Hal,
I suspect you are asking about the TLC2274 CMOS operational amplifiers.
It does not have reverse polarity protection. That is not a commom feature for analog integrated circuits. I know of only one TI operational amplifier family that does, the TLV2401 - TLV2404. The reverse battery protection is a specific design feature of these amplifiers:
http://www.ti.com/lit/ds/symlink/tlv2404.pdf
Do note that it is a very low power operational amplifier and its electrical specifications are much different than those of the TLC2274. You may not be able to apply it in all circuits where you use the TLC2274.
Regards, Thomas
PA - Linear Applications Engineering