Other Parts Discussed in Thread: PGA870, LMV7239, LMH6702
I am working with a team of engineers to design and build a time-domain reflectometer. We need to input a signal into the base of a bjt with a range of 0 to 5V. We want to use the PGA870 to control the gain on an input signal to the bjt. We decided to use the PGA870 because it has a large bandwidth and a large range of gain steps (B0 to B5). However, when prototyping it, we were getting very erratic results. We setup the circuit like the schematic on page 18 of the datasheet (single end input to differential output). When measuring the differential across the Out+ and Out- pins, we obtained at most -200mV difference. The circuit also drew around 150mA, which seems like a lot. To change the gain, we simply set gain strobe and latch mode high. The gain should then change instantaneously. We also tried toggling gain strobe high and low to set the gain. However, we weren't able to control the output with a range of 0-5V. We didn't place any resistors on the gain pins. Do we need to place resistors on those pins to limit the current into the gain pins? Could this be why there is so much current being drawn? We are also applying 5V to the gain pins to set them high. Is this okay?