pls see following schematic:
customer use LM2904 in negative power supply, and V+ is GND, and V- is -10V, and they found when ref voltage on Pin3(in+) great than -1.1V, then output PIn1
haven't output, so they provide -1.2V on Pin3, the output is ok at room temperature, but when test it in lower temperature(-20degree), the output is incorrect, pls help to fix it.