Other Parts Discussed in Thread: OPA656
Dear Members and Colleagues
I am having some trouble designing the APD receiver in a laser rangefinder. Currently my maximum range is only 100
feet while i need at least 500 feet target range. I feel the problem is in the APD bias circuit/receiver
I have custom designed the APD receiver using First Sensor's AD1500-9 APD and Texas instruments OPA656 transimpedance amplifier. My TIA
receiver has 20 Mhz bandwidth and 20Kohm gain which seems reasonable for rangefinding application.
However, I am not able to operate the APD at maximum gain (M=100). The maximum APD gain i can achieve is
M=40 and i think that is where the problem lies. In the biasing circuit for the APD ( which is just a
series resistor of 660Kohm) on increasing the High voltage output from the DC converter, there is large voltage drop across the
series resistor which results in APD bias of ~ 147 V (M=40) whereas we need 180 V as per the datasheet to
get a gain M=100. Increasing the High Voltage outapd_bias_circuit.pdfput further (upto 300 V) does not increase the APD bias
voltage. Please find the attached diagram for your reference.
Since i am not well versed with electro-optical design i am struggling to figure out how to increase the
range and troubleshoot the APD receiver.Any help/suggestion/comments on this will be greatly appreciated.
Please let me know if you have any questions
Thank You!
Sincerely
Abhishek Singhal