Other Parts Discussed in Thread: INA149
Hi
I planned to use the Difference Amplifier INA149 in my next project.
My equipment must work in the temperature range -55°C / +90°C.
In the data sheet, the performance of the INA149 are specified in the temperature range -40°C / +125°C, but the operating temperature range is -55°C / +150°C.
What can I expect below the temperature of -40°C?
Which parameters will degrade outside the temperature range -40°C / +125°C ?
Thanks in advance
Best Regards
Giorgio Menzio
AVIO S.p.A. (GE Aviation)