Hi,
Sorry, if this is not the appropriate forum for my question,I am using ASLK PRO, I want to use the kit in single supply battery powered mode(9 volts). My ultimate goal is to implement an electret microphone preamp using this kit, so that I can analyse the audio using an MSP430 kit. However, there are other opamps specifically designed for audio applications, I want to use ASLK PRO. I have gone through some video by Dr. Steven Bibyk available on TI website, he states that the ASLK kit can be used in single supply mode.
I have used TINA for simulation of TL082 in single supply mode, and run the dc and transient analysis, so far simulation results are correct, but when I switch to ASLK hardware, nothing seems to work.I am attaching the TINA model.