OPA 657: What is the output impedance of the amplifier without any load connected at the output. I went through the datasheet and cannot find the value.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Al,
Closed-loop output impedance of OPA657 is in the data sheet (see below) and the open-loop output impedance may be simulated using the existing spice macro-model (see the attached file for procedure). At lower frequency, Zout seems to be around 7.6ohms (assuming the macro-model itself is correct).