Other Parts Discussed in Thread: OPA2277, TLC2652
Colleagues
our customer Mekhanotronika reports of problem with OPA2277 amp.
As they say, there are high frequency (>100MHz) oscillations of small magnitude (<1mV). If they load 100pF cap, the oscillations disappear. It is critical for them as they use 16ch amps then MUX and ADC. The oscillation from one channel deliver changing signal in another channel.
Now they test the system and they are not sure to use OPA2277 in serial production.
Is there any information concerning such OPA2277 behaviour? They can use some AD867x instead our OPA.
BR
Alexander Kazakevich