I have the following questions related to the XTR111 datasheet. The intent of clarifying these questions is to document the expected accuracy of a system, which uses the XTR111 as a part of that system. I have found other E2E threads that discuss linearity errors, in particular this one. Your assistance is appreciated in addressing the questions below.
I need some help defining electrical characteristics in the XTR111 datasheet. The datasheet lists nonlinearity error (defined as Iout/Iset) as 0.02% of span, and then something called ‘span error’ (also defined as Iout/Iset, although with a different footnote).
First question : I would like to know what the definition of span error and nonlinearity errors are. It is not clear to me. My best guess is that span error is similar to a gain error, but I am not sure. Defining both nonlinearity and gain error for a digital device like a DAC makes sense. But I am not sure I understand it for an analog device like the XTR111. It seems like a gain error would be enough to specify the accuracy. So in essence, I do not think that I understand these terms as used for theXTR111 and would like clarification.
Second question : are the offset, nonlinearity, and span error in the XTR111 independent of each other? If they are independent, I could take the square root of the sum of squares to calculate the total error. If not, then I have to add them.
Third question : the 2011 datasheet, on page 13, states that the !EF flag is pulled up to 5V. I do not understand where the internal 5V comes from, I see nothing else in the datasheet that generates 5V. Is it pulled up to some other voltage like Vsp or Vregf, or is it really 5V?