This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS6204: Can this device be treated as a quad amplifier?

Other Parts Discussed in Thread: THS6204, THS3092, THS3091, THS3096, THS3095

Can this device be treated as a quad amplifier?
 In other words can I use the four amplifiers individually for independent functions rather than a dual differential line driver.
 Can I use them in lower gain settings than 10V/V  and maintain stability?
 To prevent oscillation what is the best location for a band-limiting capacitor besides across the supply voltage?
 Regarding the Bias settings I am trying to understand their function.
 I assume its for power conservation.
For maximum output drive capability should I use the full bias mode?