Other Parts Discussed in Thread: THS4052, OPA2312
Hello
My customer intends to use THS4052 for peak detector.
Anyway , if the input signal is large, the input signal has distortion.... attached Fig1
In case amp were OPA2312, it works well .
We( customer and I ) had two questions and I attached the schematic Fig 2
(Q1)
Please adivse the root cause of this phenomenon:: looks like large ( 3mA) bias current flowsinto in- pin
and from the in+ pin , in case input signal is large.
I think this is due to the limitation of Differential input voltage +/- 4V described in the THS4052 D/S page 2.
But I could not find the current path from IN- to IN+ in the THS4052 D/S page14 simplified schematic.
How do you think about this?
(Q2)
Do you think the current flows intenally? Is there back to back diode inside in the THS4052?
At least, We want to know THS4052 had back to back diode inside or not.
Best Regards