This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA326 current sensing

Other Parts Discussed in Thread: INA326, TIPD104

Hello,

I want to sense the output charging current of the mobile charger and convert it into a corresponding voltage. Current is in the range of 4 to 6 mA and I expect the voltage to be in the range of 4 to 5 V. My circuit operates at 5V. I found INA326 as one option, is it the right choice, if yes then could suggest me the right circuit design. I have found a document explaining the circuit diagram of INA 326, is this the appropriate circuit for me?slau504.pdf