Other Parts Discussed in Thread: ACF2101, LM741
Hi there,
I am having some problems getting the ACF2101 switched integrator to integrate. I've tried my best to troubleshoot but couldn't figure it out and am hoping that someone here can point out my mistake or give me some advice. I have it connected basically as in Figure 12 (Using the ACF2101 with a Voltage Source) in the datasheet, except that R1 is connected to 1V out from a potentiometer which is connected to +5V supply. Also, I have do not have capacitor C1, but I have a Schottky diode for D1 (1N5819, tested forward voltage drop of 0.02V)
http://focus.ti.com/docs/prod/folders/print/acf2101.html
I have the select, hold and reset pins controlled by a PIC microcontroller (outputs 3.3V), and it is powered by +-5V supply.This SOIC chip is soldered onto a SOIC to DIL adaptor and connected on a breadboard for testing.
When I put it in Integrate mode, I would expect that the voltage should integrate until it reaches the negative limit of -5V. However, on the oscilloscope I only get milivolts and this voltage does not seem to change when the IC is in any mode.
In INTEGRATE mode, a HI is sent to the reset switch and a LO is sent to the Reset switch but when I measure the voltage at the pins, both voltages are at 0.29V. However, when in HOLD mode, both switches are sent HI signals and the pins will be at 3.3V.
Any ideas would be greatly appreciated. Thanks.