the LMC662 datasheet said the operating range is from +5V to +15V, it also said that the positive power supply V+ is from +5V to +15V, and the negative power supply is from 0V to -10V. if I plan to use +5V for V+ and -5V for V-, will the output in the range of +5V to +15V or in the range of -5V to +5V?
Thank you