Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INPUT IMPEDANCE OF ISO122U

Other Parts Discussed in Thread: ISO122

I'd like to know the INPUT IMPEDANCE of ISO122U, Precision Isolation Amplifier. There is a '8.2. functional block diagram' at page 8. Looking at Vin, I'd really like to know input impedance of inner OPAMP, A1. Not 200k of series resister.

  • Hello Jong han Lee,

    We do not have any characterization data on the input impedance of that node. Please note that it is not accessible and cannot be measured from the pins of the IC. In general, the input impedance of A1 is much larger than 200 kohm but we cannot provide any specific number as such impedance cannot be characterized.

    Could you help me understand how the input impedance of A1 plays a role in your application? Maybe I can provide some additional thoughts to help you in your circuit design.

    Best regards,

    Jose

  • As Analog input, Our client required Input impedance should be at least 10MOhm.

    if not so, we should consider suitable voltage range for lower impedance than 10M.

  • Hello Jong han Lee,

    The input voltage range of the ISO122 is +/-10 V (for a VS2 supply of +/-15V).

    Best regards,

    Jose