Dear Sirs,
My Customer asked me that specification of VOH, VOL on TL974-Q1.
In TL974-Q1 data sheet, conditions of VOH and VOL of value is not listed only 25 ℃.
Some in what will VOH VOL of value in other temperature conditions other than the 25 ℃ (Full range)?
Customer conditions of use are as follows.
Vcc=3.3V (Single End)
temperature conditions :-20℃~85℃
Best Regards,
Y.Hasebe