Other Parts Discussed in Thread: ISO124, ISO120
Dear Forum Community,
I am planning to use ISO-124 isolation amplifier for DC line isolation with 1V/V gain. But I have two supply voltage to ISO124 that input voltage is 28V DC and output supply voltage is 12V DC. But Our voltage sources supply unipolar voltage. I'm not sure exactly, ISO-124 are working with Bipolar voltage supply. But I don't convert voltage sources from Unipolar to Bipolar type using external components. Also I am thinking to use 28V DC for Vs1 and 12V DC for Vs2.
At this configuration, I want to monitor input supply voltage(28V) . I am using voltage divider for input voltage monitoring. Input voltage's GND and ADC's GND are isolated by DC-DC converter. So I want to use ISO-124 for monitoring signal from Voltage Divider to ADC. Measurement accuracy is not very important to me. Tolerant can be high value. But Gain that between input and output must be 1 V/V. Could you please help me this problem solution? Could you suggest reference design for our design? My reference desing is showing in the picture below.