Other Parts Discussed in Thread: LM2917-N
What is the maximum frequency for the LM2917 with a 5V Vcc.
Thanks, David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM2917-N
What is the maximum frequency for the LM2917 with a 5V Vcc.
Thanks, David
Hi David,
fmax can be calculated using equation (4) of the LM2917-N datasheet.
fmax = I2 / (C1*VCC)
You can keep increasing the max frequency by reducing C1, but at some point, you start to lose stability and accuracy due to too small of a C1 cap.
In the EC table, linearity is specified up to 10kHz. I have not tested above this so I cannot comment on what the linearity will look like beyond that frequency.
Tim