This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Samir,
Thank you for confirming it. I was afraid I had somehow broken it or was confused. I look forward to the new device.
Is there a specific ordering code to ensure getting the new version through distribution channels (e.g. Mouser or DIgikey)?
I guess the existing device is still useable with lowpass filtering of the output. Most users probably haven't noticed the issue, since I didn't see any mention here yet. But, do you have any comment whether this high frequency oscillation might cause trouble with signals within the intended passband up ~130 MHz. I suppose nonlinearities could mix this oscillation with the input signal. Is it safe to ignore the possibility? To be specific, do you expect I can measure a 15 uA pulse signal with 0.1% resolution, given the 15 nA rms noise level (with no input) as given in the datasheet.
Thanks,
Gerard
Hello Gerard,
When the new deivce is released existing customers will receive a change notification from TI and all old inventory will be flushed so you will only receive new material.
As you mentioned the old device can be used with an LPF which is usually the case since the subsequent stages may contain an ADC which would require anti-alias filtering. I personally havent seen much of an issue with mixing that causes excess noise in the region of the amplifers BW. The 15nA rms noise level spec in the datasheet is for a limited BW up to 90MHz, so with a 1st or 2nd order low pass filter that should be achievable. This device tends to be utilized in OTDR like applications, which utilize a lot of averaging which further reduces the noise. Note that a large percentage of the output noise from the amplifier is actually caused by the 20KOhm feedback resistor.
-Samir