Other Parts Discussed in Thread: TLE2022A-EP, TL072, TLE2022
Dear Mr. Ronald Michallic, please answer
Some time ago I asked concerning TL072. I need to use it is single supply operation with supply 35V. You reported that, if I need more voltage, then I can use TLE2022A-EP (up to 40V) . Yes, 37V it is better for me. There is TLE2022AMD in Farnell catalog. Please, report, can I use TLE2022AMD with single supply 37V?
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by7318.TL072 80mA.TSC