Other Parts Discussed in Thread: XTR110, XTR111
Hello everyone!
I want to buy this device XTR110 to build a Voltage to Current Converter.
I already have the Voltage range from 0V to 5V that will be used as Input. (in fact, I tried to convert this voltage in current by using a simple BJT NPN Transistor as a current source controlled by voltage, but it didn't work as expected).
In the Output, I'm using a PLC to receive and read the 4-20mA signal, but the idea of my project is use other receivers with Resistance from 100 until 500 Ohms, and the current should be stable.
The datasheet of XTR110 specifies a typical RL of 250 Ohms in output (Figure 1). My question is: if use a power supply about 20V and use a device in the output with load resistance until 500 Ohms, the output current will be the same?
Thank's!