Other Parts Discussed in Thread: INA326, INA126
I am using an INA126PA to monitor the voltage difference between two photodiodes. The one photodiode is used as a light reference. I hooked up two INA126PA instrumentation amplifiers in the way indicated in the data sheet (http://www.ti.com/lit/ds/symlink/ina126.pdf)
V+ = 2.85V, V- = Vref = 0V. Rg = 20kohm to start such that G = 9. Vin+ and Vin- are expected to receive a signal between 0V and 0.55V depending on lighting conditions. I was expecting that when Vin+ = Vin- that the output signal Vo would equal 0. However, no matter what I put as an input signal in Vin+ and Vin- the output is always 2.11V. This is the case even if I tie Vin+ to Vin- to Vref.
For example, if Vin+ = 0.09V and Vin- = 0.06V the output should be be 0.27V, however, Vo is still 2.11V.
Do I require two power supplies to run this chip correctly?