I had some questions regarding T.I. part# OPA2354AQ1. The company I work for wants to develop an Application Note for a Single Power Supply Transimpedance Amplifier which uses one of our company's optocouplers along with the OPA2354AQ1. When testing the circuit (schematic below) with a voltage pulse coming from the optocoupler (only photodiode is shown on schematic), the OPA2354AQ1 outputs a non-biased pulse signal very similar to the input when its output is expected to be a 2.5V biased inverted pulse. And the strangest thing, when the VCC is removed from Op-Amp it still outputs the non-biased pulse, like it is being shorted. I am testing on a breadboard, I used a DIP Adapter purchased from T.I. for the OpAmp. I thought maybe I shorted some of the pins together when I soldered but so I checked resistances between the pins and that does not seem to be the case. I am looking for any advice as we are set on creating this application note using T.I. part# OPA2354-Q1