Other Parts Discussed in Thread: INA195
I need to measure high side current in a 80V nominal application. I will need 20V headroom above 80V to accommodate surge overvoltages, power supply tolerances etc. Maximum common mode in this application is 100V.
The INA195 has a maximum common mode of 80V, but the data sheet states that this voltage can be exceeded as long as the current input to any pin is limited to 5mA or less. There is no further guidance I have found on how means to achieve this and how accuracy and bandwidth is affected. Does anyone know if the common mode can indeed be exceeded on this part and the methods to do so?
Thanks