This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA122 Absolute operating temperature

Other Parts Discussed in Thread: INA122, INA126

Hello,

for an application I need to use INA122 in a oven at 85°C.

Datasheet says that the range of absolute operating temperatue is -40 to 125°C, but the same datasheet says that INA122 is specified for -40 to 85°C.

Is it possible make INA122 work at 85°C? (It doesn't matter the derating of some parameters)

Thanks.