Other Parts Discussed in Thread: LMP7715
I built up a peak detector circuit using the LMP7715. However, it's not working as expected.
Before I get into the circuit itself, my question is whether or not this choice is reasonable.
I need rail-to-rail input and output, so this helps limit the choice of amplifiers. Then, since it must drive a capacitive load through the diode, that determines some aspects of the output. I went with the LMP7715 because it was already used elsewhere in the design.
So, is this a reasonable choice, or should I immediately go elsewhere?
The application needs to capture the peak of a pulse of a ion detector. Measuring the value of the peak will determine the energy of the ion.
Thanks.