Other Parts Discussed in Thread: INA226
Hi.
I am trying to use an INA226 to sense current up to 60 amps. I have programmed the configuration data as per the datasheet but I am not getting any readings above 32.767 amps. The shunt voltage is always at it's maximum 0x7FFF. I am using four 0.01 ohm resistors in parallel (0.0025 ohm) as a shunt.
The configuration values I am using are:
CAL: 0x0400
Current LSB: 0.002
I am sure of the configuration values I obtained as the sensor works perfectly below 32.767 amps.
Am I just missing something with regards to the configuration, do I need a different shunt resistor or can this sensor not read about 32.767 amps?
Any advice would be greatly appreciated.
Thanks.