Other Parts Discussed in Thread: OPA454
I am hoping to read the status of the opa454 using a 0-5V ADC, if i have the E/D com wired to my digital ground, instead of wiring status flag to V+ through a pull up resistor, could i apply 5V, or around 7V to the status flag pin through the pull up resistor? This would be an attempt to have roughly a 5V output when there is an alarm, instead of have the alarm signal being around 90V? I would have done a simple voltage divider, but my V+ will be changing for my application, so instead of writing some software to work with an alert that will have a changing voltage level through a voltage divider, it would be great to just have a 5V output for the alarm.
-Ryan