This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LVDT Conditioner

Hello guys,

We have lots of industrial applications that use LVDT transducers to measure displacement, usually in microns.

We are considering start developing conditioners for such equipments.

The technical specs of one of this transducers is this:

Sensitivity: 7.38 mV/(Vmm)
Setting 1:10
Amplifier input load: 2 kOhm Input resistance, ± 0.1%
Supply voltage: 3.0 V ±0.5%RMS
Drive frequency: 13.0 kHz ±5%
Coil scheme: Halfbridge, TESA® compatible
Can you guys point me to a component that we can start our development? The end result shoud be a precision amplifier/conditioner that could translate this kind of signal and output it as 0..10VDC or 4..20mA with a sample rate equal or higher than 200Hz? The precision we expect, converting the signal, should be lower than 1 micron.
Thanks.