Dear Support,
I have the following requirement to compare with on the schematic attached.
whenever PSA_PSOK fall below or in the range of 2V to to 2.5V (3.3.V signal), I want to assert "PSA_PWRGD" high.
The circuit attached is not stable and some times it oscillated. I think because the Hysteresis is too small.
The vref is at 2.8V and the the power in is about around 3.3V.
Based on the formula, Vin1 and Vin2 are very closed too each other. I think they need to be half between VIN1 and VIN2. Is that right?
| VCC | R1 | R2 | Vref | Vin1 | Vin2 | |
| 3.28 | 10000 | 1000000 | 2.78 | 2.8078 | 2.775 |
What is your recommendation to change the circuit to stabilize and meet the specs requirement of < 2.5V and flag.
Thank you.
Randy