This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA210-215 EVM has no output

Other Parts Discussed in Thread: INA213, INA210

Hello,

I am receiving no output from the EVM module.

I am trying to evaluate the INA213 current sense amplifier using the Evaluation Module (INA210-215).  Here is the setup:

Using 2 DC supplies and a Signal Generator set at -20dB to attenuate down to 20mV

V+ = 5V

Vref = GND

V- = GND

Vin+ = 20mVAC rms @ 60hz  No DC offset.

Vin - GND (Return side of Signal Generator)

Ad = 50

Trying to evaluate without a shunt, but not seeing the expected output using this IC.

I have tried other IC in this family INA210 with the same results.

Goal is to see a 60hz Sine wave at 1V rms. 

Any help would be appreciated.

Respectfully,

Andy Elhardt