Can anyone explain how virtual short of the two input terminals of op-amp works?
We say that the voltage at two terminals are assumed to be the same, ie V1=V2 and then that output is A(V2-V1).
If V1=V2, then how do we get any gain at all?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can anyone explain how virtual short of the two input terminals of op-amp works?
We say that the voltage at two terminals are assumed to be the same, ie V1=V2 and then that output is A(V2-V1).
If V1=V2, then how do we get any gain at all?
Hello Ankit,
We explain negative feedback, loop-gain, and closed loop gain in both the bandwidth and stability videos of the TI Precision Labs videos (links below).
Basically the resistive feedback network in a non-inverting or inverting amplifier forms a voltage divider from the output to the inverting input. The voltage divider results in an attenuation (β) of the output voltage at the inverting input. The output must therefore equal a voltage higher than the input voltage by the inverse of the attenuation (1/β). This is how the feedback network forms a controlled closed-loop gain.