I would like to interface the XTR115 to a standard 3.3V or 5V MCU pin with PWM(isolation required). can any one provide working circuitary?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shiv,
I am moving this post to the amplifiers forum as they have answered questions related to the XTR117 in the past.
Hello,
See parts 4 and 5 of a recent blog series we published on 2-wire 4-20mA transmitters. Both blogs show a solution using the ISO7310 to properly isolate a PWM input signal for use with 2-wire 4-20mA transmitters such as the XTR115.


Hi Collin
What is the minimum impedance required after a pwm filter, to be sure not to interfere with the XTR115 input impedance?
Furthermore I'am having trouble with our XTR115 it gives an 31mA output, when trying to give it a input on Iin, if Iin pin is left floting the XTR115 output is normal. When the input on Iin is only 40µA from a 60k ohm resistor connected to Vref it also outputs 31mA?
Kind regards Willem
As shown in the blog and mentioned in some other posts you'll need to buffer the output of the passive PWM filter otherwise it will alter the input impedance of the XTR circuitry.
Also, please open a new thread for your other XTR115 questions.