Other Parts Discussed in Thread: LMV721
Hello,
This question is in regards to an LMV721 in a 3.3V single supply AC coupled inverting amplifier configuration with the non-inverting reference near 0.3V. Questions arise since the AC coupled signal will force a signal input that could exceed the maximum rail input voltages but will be current limited by 10k series R (I in/out max <500uA). Will this damage the amp? Why is there not a maximum input current limitation on the datasheet like many other amplifier datasheets? Thank you very much.
Russell