Other Parts Discussed in Thread: TLV2772, TLV2771
Hello All,
I'm trying to make a PCB for a charge amplifier of a piezoelectric device using the circuit shown below. However, I'm using 1x TLV2771 (for buffering the 1/2VCC) and 2x TLV2772 (I'm using 4 piezoelectric devices, and I'm using one TLV2772 for each pair). I'm using the same Rf and Cf for all sensors, but for some reason, I'm getting 2 difference output voltages from the TLV2772's. For example, one TLV2772 is showing 1.78V and 1.69V at the output pins while the other TLV2772 is showing 2.21V and 2.12V! The crazy thing is that I made this exact circuit on a breadboard, and the voltages were all the same at the TLV2772 output pins (1.69V). In fact, on my breadboard, I used no decoupling capacitors and no effort to shield wires.
Is there something about the 8-SOIC package that I need to consider when designing/fabricating my board? I checked the resistance, capacitance, and 1/2VCC values of the charge amplifier circuits, and they all appear to be roughly the same for all op amp circuits (22Mohm, 1nF, and 1.41V respectively).