Other Parts Discussed in Thread: TLV2372
Hello,
Will the TLV2372 op amp invert the output phase if input exceeds the supply rail?
Thank you, Keith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV2372
Hello,
Will the TLV2372 op amp invert the output phase if input exceeds the supply rail?
Thank you, Keith
Hi Keith,
The TLV2372 input stage is designed not to phase inversion. The Absolute Maximum Ratings list the common-mode voltage (CMV) range from (V-) - 0.2 V to (V+) + 0.2 V over which the output does not phase invert. The inputs have ESD diodes to each power supply rail and will begin to conduct if one pushed the voltage beyond that range. Even then it is unlikely that the output will phase invert, but we make no assurances about device operation when the Absolute Maximum Ratings are exceeded.
Regards, Thomas
PA - Linear Applications Engineering