Other Parts Discussed in Thread: THS4509, ADS4249
Hi,
My customer is thinking to use the THS4509 with ADS4249.
I would like to confirm load component values.
The output voltage is 1.4V(typ) @VDD=+5V on THS4509, and the output voltage range is 1.1V~3.9V when the common mode voltage is 2.5V
Whereas the input voltage range of the ADS4249 is 2Vpp.
When RL=200Ω, Ro=49.9Ω, Rot=100Ω the dividing ratio is 0.5, and the amplitude is 1.4Vpp.
Is it correct understanding how to set load component values?
Please let me know if there is lack of information.
Regards,
Kuramochi