Hi,
Please provide the output voltage (VOH) Min, TYP & MAX(@ V+ = 5V). Currently in the datasheet the value is been available for V+ = 26V as shown in below figure.
Best regards / Mit freundlichen Grüßen
Girish BG
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please refer to the latest datasheet online --> http://www.ti.com/lit/ds/symlink/lm158.pdf
You can use Vcc - 1.5V for the min.
Hi Andrew,
Thanks for the response.
Here i have a situation that the output signal of my op-amp (LM2904) will be connected to the GPIO of Micro-Controller.
Consider a my minimum output voltage is (VCC-1.5V) = 3.3V - 1.5V = 1.8V.(op amp output)
And the minimum voltage to detect as high from the Micro-Controller is 0.65 x VCC = 0.65 x 3.3 = 2.145V.(Micro-Controller Input)
Please let me know at which condition my op amp will be at minimum level of VCC - 1.5V.
Regards,
Girish BG