Hello,
I'm hoping someone could clarify this for me - and I apologize that there are some basics missing on my part.
I have a single-ended sensor - let's call it an antenna. I'm pickup up random noise in addition to the signals of interest. Yes, I realize DSP processing etc, can help, but I want the design to be good from the input and forward.
The question: can connecting a device that's inherently a single-ended device, where one end currently connects to ground, be this connected in differential to help reject spurious noise signals that enter that sensor? I am hoping so.
For this task, I am looking at one of the INA series TI amplifiers. However, there are 2 constraints. One, the power supply must be single, +/-3.3 to 5V, and the other is, the sensor requires input tuning with a capacitor parallel with it, to ground.
Can someone provide some guidance on my questions?
Thanks so much!