Other Parts Discussed in Thread: XTR105, XTR117
I have a design using the XTR105UA that measures ambient temperature and I need to find a replacement that can handle ambient temperatures of up to 115C so ideally a 125C rated part. Accuracy is not as important as being able to work at the ambient temperature.
I've checked the parts from IT but I don't see any that are rated for this working temperature.
I need to find a solution that has a small board space as this is installed in a sealed enclosure that has an internal diameter of 25mm. As a test I ran the current design above the working temperature and it failed at 97 deg C.