This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM211D Operating Temp Datasheet inconsistency

Other Parts Discussed in Thread: LM111, LM211, LM311

Section 8.1 Description seems to be a misprint/typo -25 to 85C.: The LM211 is identical to the LM111, except that its performance is specified over a 25°C to +85°C temperature range

 

page 22 shows all versions of LM211D, all are -40 to 85C

LM211D        ACTIVE SOIC D 8 75    Green (RoHS & no Sb/Br) CU NIPDAU Level-1-260C-UNLIM -40 to 85 LM211

LM211DE4    ACTIVE SOIC D 8 75    Green (RoHS & no Sb/Br) CU NIPDAU Level-1-260C-UNLIM -40 to 85 LM211

LM211DG4    ACTIVE SOIC D 8 75    Green (RoHS & no Sb/Br) CU NIPDAU Level-1-260C-UNLIM -40 to 85 LM211

LM211DR      ACTIVE SOIC D 8 2500 Green (RoHS & no Sb/Br) CU NIPDAU Level-1-260C-UNLIM -40 to 85 LM211

LM211DRE4 ACTIVE SOIC D 8 2500 Green (RoHS & no Sb/Br) CU NIPDAU Level-1-260C-UNLIM -40 to 85 LM211

LM211DRG4 ACTIVE SOIC D 8 2500 Green (RoHS & no Sb/Br) CU NIPDAU Level-1-260C-UNLIM -40 to 85 LM211

 

page 4 Recommended Operating states:  LM211 as -40 to 85C, LM211Q is -40 to 125C:

 

Page 5 footnote (1) states:

Unless otherwise noted, all characteristics are measured with BALANCE and BAL/STRB open and EMIT OUT grounded. Full range for LM111 is –55°C to 125°C, for LM211 is –40°C to 85°C, for LM211Q is –40°C to 125°C, and for LM311 is 0°C to 70°C.

add: Also, on the Product Selection guide (Compare) the LM211 does not have the STROBE feature shown, so it will not show up if comparing devices with a STROBE pin.