We have a PCB board which seems to be working without the LM358. The technicians believe they do not need the LM358. Is the LM358 used for the buzzer or for the sensor? The sensor is the most critical component for the PCB board. The buzzer seems to be used for aesthetic purposes like leather in a car. The buzzer is part # YMD12095G-5V. The sensor is TS-23AP-X. Any opinions?