Other Parts Discussed in Thread: INA114
I am working with ina114. I used two individual 9V batteries (unregulated) as power sources and Rg = 10Kohm. hence the gain should be 6. But when the differential voltage is 198mV, the output is -8.45V. However, if Rg (10KOhm) is removed, then the output is 198mV.
I am unable to identify the problem here. Can anyone please help me.