Other Parts Discussed in Thread: OPA170
Hello,
I have had several failures of the OPA170 op amp in a SOT23 package. The supply voltage is + and - 15V.
The +input pin becomes internally shorted to the -Vcc pin with a resistance of 20 to 30 Ohms.
Also I have had -Vcc to +Vcc shorts of 52 Ohms.
What is the likely cause of these failures?
I suspect that these failures have happened when I was testing the boards with a digital scope.
Best regards,
Tim Orr