This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

minimum differential input voltage INA333

Other Parts Discussed in Thread: INA333

Hi,

I am going to use an INA333 to measure voltages in micro Volts range. The INA333 spec. document only provides information regarding common mode ranges, not differential mode.

I am looking for the absolute minimum differential voltage (between Vin+ and Vin-) for the INA333 to still be able to produce a good enough output.

Any one?

Thanks in advance.

More info:

Vcc=2.54V single ended

Vref= 1,27V

Voffset on Vin+: 1,27V

Voffset on Vin-: 1,27V

Input frequency: 50 Hz

Gain: 1000